cancel
Showing results for 
Search instead for 
Did you mean: 

TouchGFX without Tearing pin

PhilZalkin
Associate II

Hello,

Is it possible to use TouchGFX with a screen without TE or FMARK pin in FMC or SPI mode?

Do you have an example? THANKS

1 REPLY 1

Hello @PhilZalkin ,

I think it should be possible, but you have to provide something similar to Tearing Effect signal based on a hardware clock and with proper intervals to call OSWrappers::signalVSync() so, the TouchGFX engine can start rendering the next frame. You can read more about the process here.

Best regards,

Mohammad MORADI
ST Software Developer | TouchGFX