2021-11-02 11:22 AM
Hello,
I am trying to work with touchGFX with an SPI screen. I can properly send an image to the screen manually, so I am confident that my screen driver is working fine.
I have set a timer for the Vsync that call the touchgfx::OSWrappers::signalVSync(); function. In the main loop I call the MX_TouchGFX_Process(); and in debug it seems that the TouchGFXHAL::flushFrameBuffer function is never called so I can never send the framebuffer to the screen.
I am a bit stuck in my understanding. Is there anything special that I am required to do? I followed the information in the official website (https://support.touchgfx.com/docs/development/touchgfx-hal-development/scenarios/scenarios-fmc) and I have searched online for solution without more success.
Thank you by advance,
Regards,
Augustin
2021-11-02 12:11 PM
Selecting the custom or FMC display interface also requires developers to implement a custom TouchGFX Application Tick driver that signals
OSWrappers::signalVSync()
to unblock the TouchGFX Engine Main loop. Usually, displays used along with MCUs that have no TFT Controllers can provide a Tearing Effect signal that is connected to the MCU.
Maybe your timer dont setup ok, you checked ?
2021-11-03 2:01 AM
Thank you for your answer.
My timer is set to 4Hz and is working just fine, the OSWrappers::signalVSync() is called and the vsync_sem flag is set to 1.
And in the touchgfx_taskEntry() the OSWrappers::isVSyncAvailable() returns true so it seems to be alright
My screen does not have a TE signal that is why I am using a timer.
2021-11-22 5:15 AM
I still have the same problem. The SPI driver is working fine as well as the timer fot the VSYNC but the flush frame buffer is never called.
I have tried with different settings such as simple and partial buffer.
I am now trying to go from touchgfx version 4.17.0 to version 4.18.0
Do you have any insight on how to proceed (a bit more detailed than the documentation https://support.touchgfx.com/docs/development/touchgfx-hal-development/scenarios/scenarios-fmc)
Thank you by advance,
regards,
Augustin
2024-08-31 3:15 AM
Hey @ABricout did you finally get a solution to your proble i am also stuck