cancel
Showing results for 
Search instead for 
Did you mean: 

TouchGFX Simulator not working but not giving any errors

barisubasi
Associate II

TouchGFX Simulator is not working and it doesn't give any error while creating code or running the simulator. 

I created a new project I didn't even choose a board I tried it with the "Simulator"

I want to try some ui designs in TouchGFX. I created a new project in Simulator type:

barisubasi_0-1738067612062.png

 

I just added a white box:

barisubasi_1-1738067648098.png


I generated code:

 

 

Generate Code
    Generate
        Wrote generated/gui_generated/include/gui_generated/screen1_screen/Screen1ViewBase.hpp
        Wrote generated/gui_generated/src/screen1_screen/Screen1ViewBase.cpp
        Done
    Generate Assets
        make -f simulator/gcc/Makefile assets -j8
        Done
    Post Generate
        touchgfx update_project --project-file=simulator/msvs/Application.vcxproj
        Done
    Done

 

 

barisubasi_2-1738067679171.png

 

 

I clicked "Run Simulator":

 

 

Run Simulator
    Generate
        Done
    Generate Assets
        make -f simulator/gcc/Makefile assets -j8
        Done
    Post Generate
        touchgfx update_project --project-file=simulator/msvs/Application.vcxproj
        Done
    Compile
        make -f simulator/gcc/Makefile -j8
        Done
    Run
        build\bin\simulator.exe
        Done
    Done

 

 

barisubasi_3-1738067746057.png


I tried to search for simulator.exe file in my project directory, but the file is not exist. I'm using 4.24.2 version now. 

Since there is no error. I'm lost on debugging. Thx for help.

13 REPLIES 13

I was using it. I think the issue started after I updated the app.

There must be something different on your system.Do you have a virus scanner active? It might block the simulator.
If all else fails you can try installing TouchGFX in a virtual machine as a workaround.

Kudo posts if you have the same problem and kudo replies if the solution works.
Click "Accept as Solution" if a reply solved your problem. If no solution was posted please answer with your own.
barisubasi
Associate II

I literally resetted the whole computer just to fix this...

And yes it works now. I do not know why that issue happened but after computer reset and re-installing TouchGFX Designer and Microsoft Visual C++ Redistributable Version from this link : https://learn.microsoft.com/en-us/cpp/windows/latest-supported-vc-redist?view=msvc-170

it works now. Thanks for helping!


@barisubasi wrote:

I literally resetted the whole computer just to fix this...


Reset as in reboot or reset as in Fresh install of windows?

Kudo posts if you have the same problem and kudo replies if the solution works.
Click "Accept as Solution" if a reply solved your problem. If no solution was posted please answer with your own.