cancel
Showing results for 
Search instead for 
Did you mean: 

TouchGFX Partial framebuffers, Example/Help?

MikeP
Senior

Hi,

I am using a Nucleo F401RE with ILI9341 LCD Display and Touchgfx.

I have managed to get the display working with a single framebuffer but the RAM on the MCU isnt capible of handling the full screen size (320 x 240), so i will have to use partial frambuffering- but im struggling.

Does anyone have any working working example which i could follow and get my head around or someone to peak at my code to see where im going wrong?

The code which i have attached seems to render the first few lines then stops.

Kind Regards,

Mike

1 REPLY 1
Alexandre RENOUX
Principal

Hello,

Did you solve your problem ?

/Alexandre