2024-08-21 11:56 PM
I installedTouchGFX Designer and want to add components to my project but there are only a few in the provided library. I even did not find the buttonUp that was used in the Button Example. Where can I get more components ? I want to make 3D vector figures that change angle by parameters ( I have gyroscope MPU-6050).
2024-08-29 6:44 AM
Hello @beginerGFX,
TouchGFX provides the fundamental tools to create sophisticated widgets by either combining them in a Custom Container or improve them by using your designed graphics.
You can use the assets used for creating the buttonUp to create your button; otherwise, it is an example on what can be created.
You can read about the available basic elements (widgets) here.
Currently, TouchGFX does not have comprehensive support for 3D graphics; however, you can use the Texture Mapper to achieve it.
I hope this helps you!