cancel
Showing results for 
Search instead for 
Did you mean: 

TouchGfx Graphs: Can you have more than one variable plotted?

Garnett.Robert
Senior III

Hi,

 

The TochGFX builder appears to provide for more than one variable to be plotted on a single graph:

 

2024-09-29_14-54-54.png

But looking at the API for both types of graph there is no way I can see of specifying which line to use for the data.

 

I seems obvious that the data would have to have a common x and Y range as there is no provision for mult-range scaling.

 

If you cannot have more than one variable why does the designer provide for them?

In past projects I have overlaid multiple graphs to plot additional variables, but this is extremely tedious to build and maintain.

Kind regards

Rob

0 REPLIES 0