2021-11-10 1:08 PM
Hello, I'm trying to get TouchGFX Designer 4.18 running with my H747-DISCO, but the download to the target fails every time. Thats the console output:
ST-LINK SN : 0024001E3137511439383538
ST-LINK FW : V3J8M3
Board : STM32H747I-DISCO
Voltage : 3.26V
SWD freq : 24000 KHz
Connect mode: Normal
Reset mode : Software reset
Device ID : 0x450
Revision ID : Rev V
Device name : STM32H7xx
Flash size : 2 MBytes
Device type : MCU
Device CPU : Cortex-M7/M4
BL Version : 0x90
Memory Programming ...
Opening and parsing file: intflash.hex
File : intflash.hex
Size : 3444 Bytes
Address : 0x08100000
Erasing memory corresponding to segment 0:
Erasing internal memory sector 8
Download in Progress:
±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±± 0%
ÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛ 100%
File download complete
Time elapsed during download operation: 00:00:03.315
Hard reset is performed
make[2]: Leaving directory 'c:/TouchGFXProjects/MyApplication_8'
make[1]: Leaving directory 'C:/TouchGFXProjects/MyApplication_8/gcc'
make -C C:/TouchGFXProjects/MyApplication_8/gcc/ -f makefile_cm7 flash
make[1]: Entering directory 'C:/TouchGFXProjects/MyApplication_8/gcc'
make[2]: Entering directory 'c:/TouchGFXProjects/MyApplication_8'
Converting images
Reading CM7/TouchGFX/application.config
Generating CM7/TouchGFX/generated/images/src/__designer/image_Blue_Buttons_Round_Edge_small.cpp
Generating CM7/TouchGFX/generated/images/src/__designer/image_Blue_Buttons_Round_Edge_small_pressed.cpp
Generating CM7/TouchGFX/generated/images/include/BitmapDatabase.hpp
Generating CM7/TouchGFX/generated/images/src/BitmapDatabase.cpp
make[2]: *** No rule to make target 'CM7/TouchGFX/assets/texts/texts.xlsx', needed by 'CM7/TouchGFX/generated/texts/include/texts/TextKeysAndLanguages.hpp'. Stop.
make[2]: Leaving directory 'c:/TouchGFXProjects/MyApplication_8'
makefile_cm7:49: recipe for target 'all' failed
make[1]: *** [all] Error 2
make[1]: Leaving directory 'C:/TouchGFXProjects/MyApplication_8/gcc'
../../gcc/Makefile:10: recipe for target 'flash' failed
make: *** [flash] Error 2
Failed
2021-12-06 3:17 PM
I have almost exactly the same problem. It seems to be related to a change in TouchGFX Designer 4.18.x where they switched from using XLSX to XML formats to store text/string information. I am using a STM32H745I-DISCO. The examples work fine (just tested the up/down buttons one), but when I try to make my own (extremely simple) project I encounter the
make[2]: *** No rule to make target 'CM7/TouchGFX/assets/texts/texts.xlsx', needed by 'CM7/TouchGFX/generated/texts/include/texts/TextKeysAndLanguages.hpp'. Stop.problem you observed. I'm guessing there's a template that needs to be updated (by ST). If you roll-back to version 4.17.x does it work?
I noticed another weird thing (maybe normal...I'm not familiar enough with TouchGFX tools to know for sure): the file mentioned in the log seems to get generated momentarily then removed. I made a copy of it before it got removed, and it doesn't even appear to reference the XLSX files.... Here's what my CM7\TouchGFX\generated\texts\include\texts\TextKeysAndLanguages.hpp file looks like (I defined a second language called "Other" while troubleshooting, but you can ignore that)
/* DO NOT EDIT THIS FILE */
/* This file is autogenerated by the text-database code generator */
#ifndef TOUCHGFX_TEXTKEYSANDLANGUAGES_HPP
#define TOUCHGFX_TEXTKEYSANDLANGUAGES_HPP
enum LANGUAGES
{
GB,
OTHER,
NUMBER_OF_LANGUAGES
};
enum TEXTS
{
T___SINGLEUSE_172W,
T___SINGLEUSE_8H44,
NUMBER_OF_TEXT_KEYS
};
#endif // TOUCHGFX_TEXTKEYSANDLANGUAGES_HPP
2021-12-06 3:22 PM
I tried creating a blank XLSX file for `CM7\TouchGFX\assets\texts\texts.xlsx` and this seems to make that error go away!
2021-12-06 3:24 PM
Instead I see a (presumably harmless):
WARNING: Using "CM7/TouchGFX/assets/texts/texts.xml" instead of "CM7/TouchGFX/assets/texts/texts.xlsx"