2024-04-03 12:58 AM
Hello,
I am using the TouchGFX designer to create project and source files , afterward import the project to CubeIDE.
I am using TouchGFX 4.23.2 and CubeIDE 14.1 .
I've seen many question regards this topic , but surprisingly none of the advices solves this very basic problem for me.
After creating the sources in TouchGFX, I am opening the CubeIDE workspace in the project root (not inside CubeIDE folder.
From that location I've tried the following:
1. File -> Open Project From File SYstem -> Directory:
Show two projects. One of the called as the TouchGFX project and the othe called CubeIDE.
None of them is exports nothing to the CubeIDE.
2. Import Project -> Existing Project Into Workspace:
Import a project that *always* called CubeIDE, although in .project file there is another name.
In addition the .ioc file has another name.
Renaming the files currently did not succeed, therefor I failed to create 'operational' project.
Please guide how should the user create a simple project in the TouchGFX designer and then import it into the CubeIDE.
Best regards,
Dotan
Solved! Go to Solution.
2024-04-14 8:06 AM
Hey Muhammad,
The TouchGFX project import together with the CubeMX project generation solved my problem.
I've created a CubeIDE project with proper naming convention on top of TouchGFX example.
Thank you very much for the detailed and professional support.
Cheers,
2024-04-16 1:56 AM
Hey,
Glad to hear I could help
Good luck