cancel
Showing results for 
Search instead for 
Did you mean: 

TouchGFX cube_programmer.mk project File template

WhyIsThisSo
Associate III

TouchGFX projects has a cube_programmer.mk in each project folder.

I have installed my CubeProgrammer in a different location to the default location in the cube_programmer.mk. I was wondering if the cube_programmer.mk is created on each project creation as part of the code within in the TouchGFX IDE or is it a file template which is copied from another location each time? I would like to change the master file so I do not have to change the project file each time.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
MM..1
Chief III

Maybe simpler is use MKLINK and create symlink on default place