cancel
Showing results for 
Search instead for 
Did you mean: 

Touchgfx bulleted text list?

CPaye.1
Associate III

I have an application where there is a potential for lots of text. It would be nice to break up the next into a bulleted list or a numbered list. Is there a clever way to do this with the Touchgfx framework?

I think making typed text values for each block will be too tedious for the amount of text I will be working with. The only other option I can think of is creating an image of the formatted text and using that.

Thanks.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
CPaye.1
Associate III

It turns out that if you use bulleted text in the Excel spreadsheet, that bullets will carry over into the text generated for the application:

0693W00000HpOhdQAF.png

View solution in original post

2 REPLIES 2
MM..1
Chief III

Maybe nobody understand without example, try show one or two onscreen texts

CPaye.1
Associate III

It turns out that if you use bulleted text in the Excel spreadsheet, that bullets will carry over into the text generated for the application:

0693W00000HpOhdQAF.png