2024-08-07 9:15 AM
When i run target this message appeared plz help me
'' Compiling Utilities/JPEG/jpeg_utils.c
Compiling Common/Src/system_stm32h7xx_dualcore_boot_cm4_cm7.c
Compiling ASM STM32CubeIDE/CM7/Application/User/Startup/startup_stm32h747xihx.s
Linking CM7/TouchGFX/build/bin/target.elf
CM7gcc/makefile_cm7:442: recipe for target 'CM7/TouchGFX/build/bin/target.elf' failed
/Middlewares/ST/touchgfx/lib/core/cortex_m7/gcc\libtouchgfx-float-abi-hard.a(LCD24bpp.o): In function `touchgfx::LCD24bpp::DecompressorRGB_QOI::blitCopyARGB8888(unsigned char const*, touchgfx::Rect const&, touchgfx::Rect const&, unsigned char)':
(.text._ZN8touchgfx8LCD24bpp19DecompressorRGB_QOI16blitCopyARGB8888EPKhRKNS_4RectES6_h+0x328): undefined reference to `touchgfx::paint::flushLine(unsigned long*, int)'
(.text._ZN8touchgfx8LCD24bpp19DecompressorRGB_QOI16blitCopyARGB8888EPKhRKNS_4RectES6_h+0x4e2): undefined reference to `touchgfx::paint::flushLine(unsigned long*, int)'
CM7/Middlewares/ST/touchgfx/lib/core/cortex_m7/gcc\libtouchgfx-float-abi-hard.a(LCD24bpp.o): In function `touchgfx::LCD24bpp::DecompressorRGB_QOI::blitCopyRGB888(unsigned char const*, touchgfx::Rect const&, touchgfx::Rect const&, unsigned char)':
(.text._ZN8touchgfx8LCD24bpp19DecompressorRGB_QOI14blitCopyRGB888EPKhRKNS_4RectES6_h+0x46a): undefined reference to `touchgfx::paint::flushLine(unsigned long*, int)'
(.text._ZN8touchgfx8LCD24bpp19DecompressorRGB_QOI14blitCopyRGB888EPKhRKNS_4RectES6_h+0x4ea): undefined reference to `touchgfx::paint::flushLine(unsigned long*, int)'
collect2.exe: error: ld returned 1 exit status
make[3]: *** [CM7/TouchGFX/build/bin/target.elf] Error 1
make[3]: Leaving directory 'c:/TouchGFXProjects/MV_Display'
make[2]: *** [generate_assets] Error 2
gcc/makefile_cm7:438: recipe for target 'generate_assets' failed
make[2]: Leaving directory 'c:/TouchGFXProjects/MV_Display'
make[1]: *** [all] Error 2
Makefile_cm7:51: recipe for target 'all' failed
make[1]: Leaving directory 'C:/TouchGFXProjects/MV_Display/gcc'
make: *** [flash] Error 2
../../gcc/Makefile:10: recipe for target 'flash' failed
Failed
Failed
''
Solved! Go to Solution.
2024-08-09 7:37 AM
i did it and it works but new errors appeared when i run on touchgfx but with cubeide when i build there isn't error : gcc/makefile_cm7:503: recipe for target 'CM7/TouchGFX/build/Riverdi_70STM32H7/CM7/TouchGFX/target/generated/TouchGFXGeneratedHAL.o' failed
make[3]: *** [CM7/TouchGFX/build/Riverdi_70STM32H7/CM7/TouchGFX/target/generated/TouchGFXGeneratedHAL.o] Error 1
make[3]: Leaving directory 'c:/Users/Aziz/Downloads/aaaaaa/MV_Display'
gcc/makefile_cm7:438: recipe for target 'generate_assets' failed
make[2]: Leaving directory 'c:/Users/Aziz/Downloads/aaaaaa/MV_Display'
make[2]: *** [generate_assets] Error 2
Makefile_cm7:51: recipe for target 'all' failed
make[1]: Leaving directory 'C:/Users/Aziz/Downloads/aaaaaa/MV_Display/gcc'
make[1]: *** [all] Error 2
../../gcc/Makefile:10: recipe for target 'flash' failed
make: *** [flash] Error 2
Failed
Failed