cancel
Showing results for 
Search instead for 
Did you mean: 

Templates folder has no files using the latest CubeMX

Trevor Jones
Senior

after running Cube for H7,

the <project folder> <template> folder has no files.

I had to copy this to make it work:

I had to copy the contents of the folder :

C:\Users\DAVE\STM32Cube\Repository\STM32Cube_FW_H7_V1.5.0\Drivers\CMSIS\Device\ST\STM32H7xx\Source/ select "Templates"

to :

C:/Users/DAVE/STM32Cube/Repository/STM32Cube_FW_H7_V1.5.0/Projects/H743-144-LCD1/Drivers/CMSIS/Device/ST/STM32H7xx/Source

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
Khouloud ZEMMELI
ST Employee

​Hello @Community member​ ,

could you please share your ioc file (where the probleme exist) ?

best regards,

Khouloud

Thanks for looking into this for me. <> Virus-free. www.avg.com <> <#DAB4FAD8-2DD7-40BB-A1B8-4E2AA1F9FDF2>

​you are welcome, attach your ioc please.

Best regards,

Khouloud

T J
Lead

I did attach it from my email, :(

now logged in,

it is the same for H7 or F7,

when using GPGSC, the templates folder is missing many necessary files.

Khouloud ZEMMELI
ST Employee

Hello ​@Community member​  and @Community member​ issue will be fixed in the next release.

Best Regards,

Khouloud.

Trevor Jones
Senior

thanks for that

T J
Lead

when is the next release ?

It will be released Week 40.

Best Regards,

Khouloud.​

Trevor Jones
Senior

I found another issue

this file is also not copied across when using GPDSC

STM32Cube/Repository/STM32Cube_FW_H7_V1.5.0/Middlewares/Third_Party/FatFs/src/option/ccsbcs.c

this file is needed for long file names.