2021-01-19 11:29 PM
There is an image button.
In Normal state, the image is displayed, and when the button is pressed, the B image is displayed.
I looked at the functions to use this function.
setBitmaps (const Bitmap & bitmapReleased, const Bitmap & bitmapPressed)
If you use this function to set the boolean bpressInfo to zero.
bitmapReleased displays A image, bitmapRressed displays B image.
And if bpressInfo is 1, bitmapReleased is B image and bitmapRressed is A image.
If the function is possible, can you show me a simple example?
2021-01-20 12:04 AM
I found a way.
Thank you for reading my writing.