cancel
Showing results for 
Search instead for 
Did you mean: 

Support to 3 lines MIPI

AMerc.4
Senior

I need a round display like this:

https://www.displaymodule.com/products/dm-tftr34-359

but all the displays i found similar to that have MIPI 3 lines. I know that some MCUs have a MIPI 2 lines connection. Is it right?

Is there a way to connect this kind of displays with mipi 3 lines? Or a method to convert 3 lines in 2 lines or another method to convert mipi 3 lines in RGB888 and using so LTDC?

2 REPLIES 2

You should make friends with this guy.. https://community.st.com/s/question/0D53W000004JuLiSAK/is-it-possible-to-drive-a-three-lane-dsi-display-with-two-lanes

https://drive.google.com/file/d/1RktX8Q5kdgVfKGAkwRWcsnvQlOkfAN38/view

Personally I think 800x800 will go down two lanes at 500 MHz (250 MHz DDR) -> 1Gbps, but I'll look at the specs.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

So, is it possible to convert the 3 Lines MIPI to 2 Lines?