cancel
Showing results for 
Search instead for 
Did you mean: 

Support for 800 x 480 LCD resolution with part no. STM32L4S7VI. Does this resolution is supported by MCU ?

VVasa.1
Associate

Hi Team

I have LCD panel with 24-bit RGB Interface and having resolution of 800 x 480. I wanted to know about its support with part no. STM32L4S7VI as its having built-in TFT Controller. I know it has 24-bit RGB support, but does it supports 800 x 480 pixel resolution ?

1 REPLY 1
berendi
Principal

Yes, but only with a reduced selection of colours, i.e. 256-colour palette mode.

The internal memory can't hold more than 1 byte/pixel at that resolution.