cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7S78-DK Flash Regions

carlos_112
Associate III

Hello!

I wonder if someone can point me to instructions on how to assign a flash memory region for TouchGFX assets on an STM32H7S78-DK, such as images and large files that won't change during an update? Currently there is a Boot and Application region setup by TouchGFX. Just need to add one for the assets so that it is not necessary to erase the whole flash and upload everything, just what is needed.

Thank you

1 ACCEPTED SOLUTION

Accepted Solutions
GaetanGodart
ST Employee

Hello @carlos_112 ,

 

You can flash only the code (not the assets) when building and flash through TouchGFX Designer :

GaetanGodart_0-1745486744011.png

Would that be enough for you to flash through TouchGFX Designer?

 

Regards,

 

Gaetan Godart
Software engineer at ST (TouchGFX)

View solution in original post

2 REPLIES 2
GaetanGodart
ST Employee

Hello @carlos_112 ,

 

You can flash only the code (not the assets) when building and flash through TouchGFX Designer :

GaetanGodart_0-1745486744011.png

Would that be enough for you to flash through TouchGFX Designer?

 

Regards,

 

Gaetan Godart
Software engineer at ST (TouchGFX)

OK, sounds good!

Thanks