2021-03-03 08:38 AM
Unzip full code
Page 49 of PDF
• Unzip the STM32H7B3Workshop2020_modified_files.7z to
the C:\2020_ST_GFX_WS\STM32H7BWorkshop2020
• It will overwrite the existing files with the implementation for all labs within
pre-processor directives #ifdef
• The modifications for each hands-on step are enabled by flags:
• LAB_STEP_1_ENABLE
• LAB_STEP_2_ENABLE
• LAB_STEP_3_ENABLE
• Description of the updated files come later here
Downloaded All from https://drive.google.com/drive/folders/11tKCY7k9lNX-Yy6uLG163kU3B3QDA-RH
Can anyone point me to the STM32H7B3Workshop2020_modified_files.7z ?
I can't find them in any of the Labs.
Thank you in Advance.
D®3W
2021-03-04 12:04 AM
Hi,
Where did you find this workshop ? I see that it was using TouchGFX 4.16 and CubeMX 5.6, which should not be an issue but still means that there will be differences with the current version of TouchGFX.
EDIT: i just realized that it is the workshop available on the ST youtube channel my bad
/Romain
2021-03-11 01:03 AM
Were you able to find it ? I did not, but it would be useful for other users as well.
/Romain
2021-07-06 01:24 PM
Was anyone able to find the archive file of the "STM32H7B3Workshop2020_modified_files.7z" referenced in page 49 of the lab document?