cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H753 LCD CONTROLLER information.

PAdam.6
Associate II

Hi Guys, I've searched the ST website on info for setting up the LCD RGB 24bit controller and can't seem to find any info. The reference manual has a little info but doesn't show pin connections etc. Is there a webpage dedicated to the LCD Controller?

Thanks Guys, Peter.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
waclawek.jan
Super User

> The reference manual has a little info but doesn't show pin connections

Those are in the datasheet.

JW

View solution in original post

4 REPLIES 4
waclawek.jan
Super User

> The reference manual has a little info but doesn't show pin connections

Those are in the datasheet.

JW

Also the examples in the HAL are limited given the number of H7 boards publicly released. You might want to pull the F7 libraries which have more examples and an equivalent controller.

See also schematics for DISCO and EVAL boards with support for parallel panels.

​

The current H7 silicon does not support DSI.

​

There are a couple of app notes on STM32 LCD​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
PAdam.6
Associate II

Thank you guys. I'll check it out. :)

SWood.8
Associate III

Succeeded in getting 128x64 parallel GLCD working on the H7. Took a lot of trial and error. It is very easy to go down rabbit holes with this technology and as someone pointed out once, there are so many variables and gotchas with interfacing that one persons 'definitely works' solution is half talent and half good luck. Can't help you in this instance but if you ever get stuck with a NT7107 / KS0106 controlled device please let me know.