cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F429 discovery board

matej2
Associate II

Has anyone been able to create a working project with CubeMX 5.5 and TouchGFX 4.13?

1 ACCEPTED SOLUTION

Accepted Solutions
Martin KJELDSEN
Chief III

Did you check the Application template from the designer?

There's a new version 3 up that supports CubeMX 5.5!

/Martin

View solution in original post

3 REPLIES 3
Martin KJELDSEN
Chief III

Did you check the Application template from the designer?

There's a new version 3 up that supports CubeMX 5.5!

/Martin

MKsen.1
Associate II

I did at first, but it wasn't there. Now I see that there is a new template version there. Thanks for posting this, and I will give it a try.

Matej

MKsen.1
Associate II

I have tried it out and if you are using the template screen transitions are not working on device (project built with cube IDE), but are working fine in the TouchGFX Simulator. Is there something that needs to be enabled?

Thx Matej