STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

change Vsync

HiI'm using stm32f429 and my question is about LTDC peripheral.Is there any way to change VSYNC unit from "Line" to "pixel"?(Like Hsync unit that is in pixel)Thanks

Resolved! Displaying mix of Chinses and English character

I want to display mixture of Chinses and English character but unable to correct find font in toughgfx.For example utf-8 encoding E4 BD A0 E5 A5 BD 20 43 68 61 6E 64 61 6E 21 is 你好 Chandan!Please let me know which font should I select at touchgfx. Th...

0693W000005A97zQAC.png

Resolved! HardFault in MX_TouchGFX_Init()

I try to make a TouchFGX demo for a self designed STM32F750 board. The board hardware is verified, it works with my "hand made" simple test image graphics. The board does not have any kind of touch input, but some hardware-buttons.And the memory layo...

0693W000001reYNQAY.jpg 0693W000001reYSQAY.jpg
TThan by Associate III
  • 4596 Views
  • 6 replies
  • 0 kudos

Resolved! Animation of 'moveTo' function

Hi, I remember that in the past I've seen in the TouchGFX documentation a function that was like the 'moveTo' function but with the possibility to have an animation from the initial position to the final position of the object. I don't remember if it...

SPano.1 by Associate II
  • 1827 Views
  • 2 replies
  • 0 kudos

TouchGFX and low power modes

Hi, I followed the touchGFX workshop today and at a certain point we had a discussion about the problem of using state preserving low power modes of the cpu in combination with running touchGFX.The example that triggered the discussion during the co...

Resolved! X-Nucleo-GFX01M1 (X-Cube-Display) and NUCLEO-G071RB issue with the demo code, unable to load and run without 'MI command LOAD...' error.

Received my GFX01M1 board to use with the Nucleo-G071RB. First, tried to load the precompiled binary in the project workspace with no luck. I get the 'Failed to execute the MI command LOAD ***.elf'. Re-compiled the code with no issue but resulting in...

TJM by Senior II
  • 1743 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.