‎2020-02-12 11:09 PM
Hello There,
I am trying to connect OV9655 camera (WaveShare) module with STm32f4 discovery board. After generating files from CubeMX and importing ov9655 drivers (ov9655.h & ov9655.c) I am able to get HAL_DCMI_LineEventCallback and HAL_DCMI_VsyncEventCallback event but not able to get HAL_DCMI_FrameEventCallback.
I am using Snapshot mode
BSP_CAMERA_Init(RESOLUTION_R320x240);
HAL_Delay(1000);
HAL_DCMI_Start_DMA(&hdcmi, DCMI_MODE_SNAPSHOT, (uint32_t)CAMERA_FRAME_BUFFER, GetSize((uint8_t *)RESOLUTION_R320x240));
Please suggest where I am making mistake. Also please let me if any further info needed.
DMA Initialization
/**
* Enable DMA controller clock
*/
static void MX_DMA_Init(void)
{
/* DMA controller clock enable */
__HAL_RCC_DMA2_CLK_ENABLE();
/* DMA interrupt init */
/* DMA2_Stream1_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA2_Stream1_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(DMA2_Stream1_IRQn);
}
/**
* @brief DCMI Initialization Function
* @param None
* @retval None
*/
static void MX_DCMI_Init(void)
{
/* USER CODE BEGIN DCMI_Init 0 */
/* USER CODE END DCMI_Init 0 */
/* USER CODE BEGIN DCMI_Init 1 */
/* USER CODE END DCMI_Init 1 */
hdcmi.Instance = DCMI;
hdcmi.Init.SynchroMode = DCMI_SYNCHRO_HARDWARE;
hdcmi.Init.PCKPolarity = DCMI_PCKPOLARITY_FALLING;
hdcmi.Init.VSPolarity = DCMI_VSPOLARITY_LOW;
hdcmi.Init.HSPolarity = DCMI_HSPOLARITY_LOW;
hdcmi.Init.CaptureRate = DCMI_CR_ALL_FRAME;
hdcmi.Init.ExtendedDataMode = DCMI_EXTEND_DATA_8B;
hdcmi.Init.JPEGMode = DCMI_JPEG_DISABLE;
if (HAL_DCMI_Init(&hdcmi) != HAL_OK)
{
Error_Handler();
}
‎2020-02-13 1:44 AM
Hi. You must initialize DMA before calling HAL_DCMI_Start_DMA. Because HAL_DCMI_FrameEventCallback rise by setting DCMI_IT_FRAME bit. (from function DCMI_DMAXferCplt, file stm32f4xx_hal_dcmi.c). Check example for STM324xG_EVAL in your local CubeMX repository.
‎2020-02-13 1:52 AM
Thank you very much for your reply. I have already did so. Please check the full main function :
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
//MaxInitDMA1();
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_I2C1_Init();
MX_USART1_UART_Init();
MX_CRC_Init();
MX_DCMI_Init();
/* USER CODE BEGIN 2 */
BSP_CAMERA_Init(RESOLUTION_R320x240);
HAL_Delay(1000);
HAL_DCMI_Start_DMA(&hdcmi, DCMI_MODE_SNAPSHOT, (uint32_t)CAMERA_FRAME_BUFFER, GetSize((uint8_t *)RESOLUTION_R320x240));
//HAL_DCMI_Start_DMA(&hdcmi, DCMI_MODE_SNAPSHOT, frame_buffer, GetSize((uint8_t *)CAMERA_R160x120));
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
//HAL_DCMI_Start_DMA(&hdcmi, DCMI_MODE_SNAPSHOT, (uint32_t)CAMERA_FRAME_BUFFER, GetSize((uint8_t *)CAMERA_R160x120));
}
/* USER CODE END 3 */
}
‎2020-02-13 2:16 AM
Did you properly initialize DMA for DCMI data fetching? Share you CubeMX file.
‎2020-02-13 2:48 AM
‎2020-02-13 3:18 AM
Configuration for DMA from STM32F4xG_Eval Example for DCMI Snapshot Mode
/*** Configure the DMA streams ***/
/* Configure the DMA handler for Transmission process */
hdma.Init.Channel = DMA_CHANNEL_1;
hdma.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdma.Init.PeriphInc = DMA_PINC_DISABLE;
hdma.Init.MemInc = DMA_MINC_ENABLE;
hdma.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD;
hdma.Init.MemDataAlignment = DMA_MDATAALIGN_WORD;
hdma.Init.Mode = DMA_CIRCULAR;
hdma.Init.Priority = DMA_PRIORITY_HIGH;
hdma.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
hdma.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_FULL;
hdma.Init.MemBurst = DMA_MBURST_SINGLE;
hdma.Init.PeriphBurst = DMA_PBURST_SINGLE;
hdma.Instance = DMA2_Stream1;
DMA Mode is CIRCULAR.
‎2020-02-13 3:22 AM
Thanks. I will change the setting from Normal to Circular & test. Will revert with results. Thanks for your prompt responses.
‎2020-02-13 3:34 AM
Refer to this document Digital camera interface (DCMI) for STM32 MCUs
"In snapshot mode: the DMA must ensure the transfer of one frame (image) from the DCMI to the desired memory:
– If the image size in words does not exceed 65535, the stream can be configured in normal mode. For more detailed description of this mode, refer to Section 4.4.6: Normal mode for low resolution in snapshot capture"
So it must works in normal mode. Maybe problem with CAMERA_FRAME_BUFFER location. Where you place it?
‎2020-02-13 3:36 AM
Memory location : 0x64000000
‎2020-02-13 4:26 AM
This address mapped to external NOR/PSRAM. You didn`t initialize SRAM in your main.