2017-02-13 7:57 AM
Hello
It is mentioned in the dcmi section of the stm32f4 electrical specification that the max pixel clock is 54MHz with 14 data lines which yields to 94.5MBps throughput, but the max throughput is said to be 54MBps in the dcmi section of both datasheet and reference manual.
#54 #94.5 #throughput #stm32f4-dcmi #confusion2017-02-13 8:08 AM
I'd agree that the documentation doesn't really account for bytes/words in a coherent fashion.
From a practical sense the sustained rate is likely to be lower as you have to process and store the data. ie your ability to capture specific frames, vs streaming a continuous sequence of frames over a second or more.
2017-02-16 7:18 AM
Hello
As i inspected through some of stm32f7 datasheet, it is clarified in dcmi section that the throughput rate is 54MBps for 8 bits of data at 54MHz. but the conflict remains as it is said in electrical section that (as in stm32f4 datasheet):
Unless otherwise specified, the parameters given in
Table 120
for DCMI are derived
from tests performed under the ambient temperature, f
HCLK
frequency and V
DD
supply
voltage... .
If the tests are really done for 14bits of data at 54MHz, the throughput rate then must be 94.5MBps. the question is what was the DMA configuration under test condition? by ignoring the cpu ability to process this amount of data rate, is this throughput rate achievable by dcmi and dma together or not?
2017-02-16 8:26 AM
The DMA, and the memory behind it, would need to sustain 108 MBps
2017-02-16 9:34 AM
You are right, 4bits in every word is unusable but must be sent, So is it able or not?
2017-02-16 10:22 AM
This isn't my project, you'll need to do some of your own validation testing to be comfortable with your interpretation of the functionality, and discuss with FAEs assigned to your account about specific corner conditions and what memories, and memory speeds would be needed for optimal performance.