cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX and STemWin

william239955_stm1_st
Associate II
Posted on January 28, 2016 at 18:01

Hi,

I want to evaluate using STemWin in a new project but for the life of me I can't figure out how to use STM32CubeMX to generate code with STemWin. From what I understand it wasn't included but now it is. The download page says it's now included. I see the libraries in the Middleware folder but no way to enable it in a project.

Am I missing something or do I need to import it afterwards in the IDE?

One side question. I was going to use the STM32F411RE would it be worth upgrading to STM32F429? I can't seem to find the difference with the 429 vs 439 either.

Thanks. 

#stemwin #stm32cube
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Nesrine M_O
Lead II
Posted on February 01, 2016 at 16:10

Hi  MobileWill,

1-''The download page says it's now included.'' which page?

2-What do you need exactly as feature to help you to select the suitable MCU?

-Syrine-

william239955_stm1_st
Associate II
Posted on February 01, 2016 at 17:48

http://www.st.com/web/en/catalog/tools/PF259225

I think I am going to go with the F429. I need a good graphical interface, sd, reading i2c sensors, and USB serial. 

Nesrine M_O
Lead II
Posted on February 01, 2016 at 18:14

Hi MobileWill,

But on this page there no indication that we can generate MX project including STemWIN library.You have to do it manually.Please refer to this [DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Java/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Java/STemWin%20and%20STM32CubeMX%20project%20integration&currentviews=934]post you find an official response from our MX team about STemWin and STM32CubeMX integration. 

You can find some working example with STM32F429 device under the STM32F4 cube firmware package: 

STM32Cube_FW_F4_V1.10.0\Projects\STM324x9I_EVAL\Applications\STemWin 

-Syrine-

william239955_stm1_st
Associate II
Posted on February 01, 2016 at 18:23

Thanks you I will give that a try. Are there plans to add it into the Cube generation? 

I also found the UI builder is buggy. Can't add the Menu element without it crashing.