cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 LTDC TouchGFX GUI Glitching

Trampler
Associate II

What could be the cause of this glitch on my LCD-TFT screen? My system includes an F429 MCU, an SDRAM, and a 24-bit LCD panel. The interface was designed with TouchGFX, and the circuit board was designed by me.

 

 

1 REPLY 1
MM..1
Chief III

Try add some real gui elements. Here you have no info relevant. Debug faults...

Or for example use two screens and setup delay and transition screen 1 to 2 and back....