cancel
Showing results for 
Search instead for 
Did you mean: 

STemWin, CubeMX and L4 family

José Miguel Matos
Associate

Hi, I am trying to create a project in CubeMX for the TrueStudio but i can not connect the round LCD(MB1314). I am using the STM32L4R9I-Eval

I already tried to use the application examples present in the Repository but I only connect to an image through DSI, but with STemWin the screen never turns on.

I need help with some example or if possible with the *.ioc file.

Thanks.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
hansd56
Senior II

Hi, there is an Hello World example at 'STM32 Repository\STM32Cube_FW_L4_V1.14.0\Projects\STM32L4R9I-EVAL\Applications\STemWin\MB1314\HelloWorld'. I hope this helps.