cancel
Showing results for 
Search instead for 
Did you mean: 

STemWin create QR_Code

zhao yongchao
Associate
Posted on May 23, 2017 at 06:46

Hi.

I'm using STemWin 5.28.

Today i was reading web page in seeger web. I find that  the lastest EMWin version is V5.40 .U

nbelievable,I find the function 

in the chapter '2-D  Graphic Library' GUI_QR_Creat(), GUI_QR_Delete()....

Now ,Which version of STemWin support QR_Code ? HOW can i get the lastest version?  

I'm using STM32f103vet6.

Best regards.

#qr_code #stemwin
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Imen.D
ST Employee
Posted on May 30, 2017 at 14:02

Hi

yongchao.zhao

,

QR-Codes functionadded in the STemWinversion 5.

Today,

the

STemWin-library is based on version V5.28 for the last version of STM32CubeF1 V1.4.0.

So,you can't use the

QR-Codes functions

since it is not available in the STemWin 5.28 with the last firmware package.

Thanks

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Posted on June 01, 2017 at 03:51

Thank you for your help. I hope ST updates the lib as quickly. Now i only use the libqrencode written by fukuchi.  

 Best regards!