cancel
Showing results for 
Search instead for 
Did you mean: 

Renaming a screen in Designer causes compilation error

Michael B
Associate III

Renaming a screen results in a compilation error.

To reproduce:

  1. Create a new project
  2. Rename Screen1 to MainScreen
  3. Run Simulator
Converting images
Compiling gui/src/screen1_screen/Screen1View.cpp
Compiling generated/images/src/slider_vertical_***.cpp
Compiling generated/images/src/pageindicator_highlight.cpp
Compiling generated/images/src/menu_stage_stretch_left_side.cpp
Compiling generated/images/src/slider_vertical_fill.cpp
Compiling generated/images/src/slider_vertical_back.cpp
Compiling generated/texts/src/LanguageGb.cpp
Compiling generated/texts/src/TypedTextDatabase.cpp
gui/src/screen1_screen/Screen1View.cpp:1:46: fatal error: gui/screen1_screen/Screen1View.hpp: No such file or directory
 #include

This discussion is locked. Please start a new topic to ask your question.
7 REPLIES 7

Hi @Community member​,

Have you added any code manually to Screen1View.cpp? If so, then we (Designer) will not delete this file since it contains additional code which is not generated by the Designer.

In this case, you should find that the gui src folder contains both a MainScreen and a Screen1View folder.

Delete the Screen1View folder and it should be ok.

Just remember to copy the handwritten code from the old file to the new.

/Anders

Nope it was a fresh project as described above, with no changes at all. I for now just kept the default names for different screens, but obviously not a great solution. I can modify the build by hand I was just surprised that such a simple and common operation didn't work.

Normally this operation works in the designer, so it does seem at bit strange, i'll report it to the designer team.

If you still have the "broken" project, please provide a list the files in the gui folder e.g. using "find gui" in the touchgfx environemnt when standing in the root of the project.

/Anders

Martin KJELDSEN
Chief III

Hi @Community member​,

I don't have that problem here. Can you please send me the project?

/Martin

wired
Senior III

This was identified as a bug in 4.18 when I submitted support case 145131 for this very issue. They said they would look into it for the next release. Well, now 4.19 is here. I have not installed it yet, so am wondering if this problem still exists? I just renamed a screen and had to go in and modify about six gui files, since all TouchGFX does is create a new set of View and Presenter files when you rename a screen. I had to manually change all of the class names and header file names to reference the new name.

I just found this thread, and I see that this bug has existed for over three years now and was not fixed as of 4.18, so I'm not holding out much hope...

Hello wired,

Unfortunately still in 4.19.0. Indeed we don't want to modify user code (we only modify generated code) because deleting/renaming theses old named files (that contains user code) is a bit dangerous. It's not just about creating new files and copy user code into it sadly. But I pushed again this issue to my team and I believe we can find a solution to this soon. We'll get back to you as soon as possible..

/Osman

Osman SOYKURT
ST Software Developer | TouchGFX

Hi Osman,

Seems to me to be no more difficult than doing a search and replace of class names and include files, and renaming of the existing files to contain the new screen name. That is what I had to do.

At the very least, if nothing is going to be done about it, you could pop up a dialog stating that changing the screen name once user code has been added may result in compilation errors, and confirm that they want to continue. It is never a good idea to allow someone's code to break by performing an allowed action in the application. You know, because of the old "just going to rename this screen before showing the boss my demo" scenario ;)