cancel
Showing results for 
Search instead for 
Did you mean: 

Problems of sources building within STM32cubeIDE

ddelt.1
Associate II

Here is my problem:

I create a STM32cube IDE project by including an additionnal software named TouchGFX . I generate the project so that it gets

with the discovery 32F469 NI card...and a windows message appears which is following: " These IPs still have some not configured or wrong parameters values [STMicroelectronics

X-CUBE-TOUCHGFX 4.13.0.

The build of the project gives some errors identified in the OSwrappers and TouchGFXconfiguration .cpp

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Martin KJELDSEN
Chief III

Can you please post the errors here?

"These IPs still have..." appears when you have "warnings" or unfulfilled dependencenies in TouchGFX Generator or other places in CubeMX

E.g. If CRC is not enabled, you'll get an error.

/Martin