2015-02-26 08:53 AM
hi
i want show a text in LCD and i use LCDTS1620A-21 and stm32f0discovery#include ''stm32f0xx.h''
uint32_t TickValue=0;
#define RS GPIO_BRR_BR_13 // RS is named as Port 13
#define RW GPIO_BRR_BR_14 // RW is named as Port 14
#define EN GPIO_BRR_BR_15 // EN is named as Port 15
void
initgpio()
{
RCC->AHBENR |= RCC_AHBENR_GPIOCEN;
RCC->AHBENR |= RCC_AHBENR_GPIOAEN;
GPIOC->MODER |= (GPIO_MODER_MODER13_0 | GPIO_MODER_MODER14_0 | GPIO_MODER_MODER15_0) ;
GPIOC->OSPEEDR |= (GPIO_OSPEEDER_OSPEEDR13 | GPIO_OSPEEDER_OSPEEDR14 | GPIO_OSPEEDER_OSPEEDR15);
GPIOC->OTYPER &= ~(GPIO_OTYPER_OT_13 | GPIO_OTYPER_OT_14 | GPIO_OTYPER_OT_15) ;
// GPIOC->PUPDR &= ~(GPIO_PUPDR_PUPDR13 | GPIO_PUPDR_PUPDR14 | GPIO_PUPDR_PUPDR15);
GPIOA->MODER |= (GPIO_MODER_MODER0_0 | GPIO_MODER_MODER1_0 | GPIO_MODER_MODER2_0 |
GPIO_MODER_MODER3_0 | GPIO_MODER_MODER4_0 | GPIO_MODER_MODER5_0 | GPIO_MODER_MODER6_0 | GPIO_MODER_MODER7_0) ;
GPIOA->OSPEEDR |= (GPIO_OSPEEDER_OSPEEDR0 | GPIO_OSPEEDER_OSPEEDR1 | GPIO_OSPEEDER_OSPEEDR2 |
GPIO_OSPEEDER_OSPEEDR3 | GPIO_OSPEEDER_OSPEEDR4 | GPIO_OSPEEDER_OSPEEDR5 | GPIO_OSPEEDER_OSPEEDR6 | GPIO_OSPEEDER_OSPEEDR7);
GPIOA->OTYPER &= ~(GPIO_OTYPER_OT_0 | GPIO_OTYPER_OT_1 | GPIO_OTYPER_OT_2 | GPIO_OTYPER_OT_3 |
GPIO_OTYPER_OT_4 | GPIO_OTYPER_OT_5 | GPIO_OTYPER_OT_6 | GPIO_OTYPER_OT_7) ;
// GPIOA->PUPDR &= ~(GPIO_PUPDR_PUPDR0 | GPIO_PUPDR_PUPDR1 | GPIO_PUPDR_PUPDR2 |
// GPIO_PUPDR_PUPDR3 | GPIO_PUPDR_PUPDR4 | GPIO_PUPDR_PUPDR5 | GPIO_PUPDR_PUPDR6 | GPIO_PUPDR_PUPDR7);
}
void
s_init()
{
GPIOC->BRR=RS;
GPIOC->BRR=RW;
}
void
s_data()
{
GPIOC->BSRR=RS;
GPIOC->BRR=RW;
}
void
delay_ms(uint32_t n_ms)
{
SysTick_Config(8000*3 - 30);
TickValue = n_ms;
while
(TickValue == n_ms)
;
SysTick_Config(8000*3);
while
(TickValue != 0)
;
}
void
s_latch()
{
GPIOC->BSRR=EN;
delay_ms(10);
GPIOC->BRR=EN;
delay_ms(10);
}
void
TimingDelay_Decrement(
void
)
{
TickValue--;
}
int
main(
void
)
{
int
k=0;
char
a[]=
''WWW.EEHERALD.COM''
;
char
b[]=
''EMBEDDED SYSTEMS''
;
initgpio();
GPIOC->BRR=RS;
//Initialize RS=0 for selecting instruction Send
GPIOC->BRR=RW;
// Select RW=0 to write Instruction/data on LCD
GPIOC->BSRR=EN;
// EN=1 for unlatch. (used at initial condition)
delay_ms(10);
s_init();
//Call Instruction Select routine
GPIOA->ODR=0x0001;
// Clear Display, Cursor to Home
s_latch();
//Latch the above instruction
GPIOA->ODR=0x0038;
// Display Function (2 rows for 8-bit data; small)
s_latch();
//Latch this above instruction 4 times
s_latch();
s_latch();
s_latch();
GPIOA->ODR=0x000E;
// Display and Cursor on, Cursor Blink off
s_latch();
//Latch the above instruction
GPIOA->ODR=0x0010;
// Cursor shift left
s_latch();
//Latch the above instruction
GPIOA->ODR=0x0006;
// Cursor Increment, Shift off
s_data();
//Change the input type to Data.(before it was instruction input)
s_latch();
//Latch the above instruction
for
(k=0;a[k];k++)
{
GPIOA->ODR=a[k];
//It will send a[0]='P' as = '0x0050' on Port A.
s_latch();
//Latch the above instruction only once. Or it will clone each character twice if you latch twice.
}
GPIOC->BRR=RS;
//Initialize RS=0 for selecting instruction Send
GPIOC->BRR=RW;
// Select RW=0 to write Instruction/data on LCD
GPIOC->BSRR=EN;
// EN=1 for unlatch. (used at initial condition)
delay_ms(10);
GPIOA->ODR=0x00C0;
// Move cursor to beginning of second row
s_latch();
//Latch the above instruction
s_data();
//Change the input type to Data.(before it was instruction input)
for
(k=0;b[k];k++)
{
GPIOA->ODR=b[k];
//It will send b[0]='E' as = '0x0044' on Port A.
s_latch();
//Latch the above instruction only once. Or it will clone each character twice if you latch twice.
}
s_init();
}
but dont work :((((((((((
plz help me
i am a beginerrrrrrrrr
#stm32f0discovery #lcdts1620a-21
2015-02-26 11:05 AM
Didn't really looking at the code.
But driving a 5.0V peripheral (LCD) from a 3.3V MCU, this can't work.2015-02-26 12:59 PM
thanks
what do you means?If possible
please explain
a little more
2015-02-26 01:19 PM
The inference is that the VOL/VOH levels are incompatible. I've not looked at the data sheet for this specific display, so honestly couldn't say one way or the other. I'm using a similar one, but it's 3.3V rated.
http://www.newhavendisplay.com/specs/NHD-0216HZ-FSW-FBW-3V3C.pdf
Other peoples register level code really isn't something I'm going to spend my time on. Would suggest you look at other implementations using the Standard Peripheral Library.Connectivity otherwise doesn't look bad, but you'd want to walk through the code, make sure the delays on the pins/signals are what you expect, and debug to understand if it's getting stuck somewhere, just not responding as expected.2015-02-26 03:14 PM
''But driving a 5.0V peripheral (LCD) from a 3.3V MCU, this can't work.''
Except my friend - for those times - when it (surely) does! Might (some) attention be paid to LCD's data manual? I extract key portion, here: