cancel
Showing results for 
Search instead for 
Did you mean: 

Nucleo-f767zi and x-nucleo-GFX02zi CubeMX and HelloWorld

Carsten73
Associate III

Hello,

 

I am new at the STM32 World. 

 

I started to buy a nucleo-f767zi and it worked fine. 

 

I was not able to get the debug Console running. Like other too. 

 

Because of that I bought the extension Board  x-nucleo-GFX02zi which should be working fine with the F767ZI. 

 

Now I tried with CubeMX to installed the Hello World Example provided.

But now I get the Message that these Packets is not Support with CubeMX 6.11. It should be support by Version 6.7 until 6.8.2.

 

I tested 6.8.2 and 6.8 but without any changes. It seams like the SPI does not fit together. Always I got no solution found. 

 

Does the GFX02zi can be used with the F767ZI? Or do I have to everything new. 

 

I am going a bit crazy. 

 

Is there anyway a working step by Step intruduction for Add a Display to a STM32. 

 

Thanks for any help 

best regards

Carsten 

This discussion is locked. Please start a new topic to ask your question.
15 REPLIES 15

Thanks. exactly. 

 

But the test and prototype no a GUI and PINs. 

 

Because of that, I bought a simple LCD SPI Display which is very good documented and Howto`s are available. 

 

I hope this way I can achieve success more quickly. 

 

Thanks 

Carsten

 

Sure, not problem. We provide our board + display setup just for easy of use.

Just out of curiosity, may I know what display you went for?

Gaetan Godart
Software engineer at ST (TouchGFX)

I bought a simply ILI9341 SPI one. 

I saw enough documentation and explanations howto.  

I am looking foward to get it running next week.

 

carsten

Oh ok.

Yes, a  lot of people use it so there is a lot of documentation about it but it is also all over the place, it is a mess. :grinning_face_with_sweat:

I personally think we should make a TBS or 2 for this display and maybe some more for other ILI9xxx.

Gaetan Godart
Software engineer at ST (TouchGFX)

would be helpful. 

 

If you like I can tell you my result, next week

GaetanGodart
ST Employee

Sure, that would help us if we end up doing a TBS for it (and that would also help me convince the product owner)!

Gaetan Godart
Software engineer at ST (TouchGFX)