cancel
Showing results for 
Search instead for 
Did you mean: 

More than one widget , how to refresh once together?

Breeze1
Associate III

In Screen, I have 3 or more widgets , they are the same type of widget, but can not make them in one container. In normal , I have to invalid one by one. Now , I need them to refresh together, how do I do?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
HP
Senior III

the refresh rate is so high that invalidating them one by one should be fine?

another option could be to update the widgets when you enter the screen. use the activate method in the presenter to do that.

Breeze1
Associate III

For low power reason, we slow down the refresh rate. Now the refresh rate is no more than 10. If invalidating one by one , it will stuck.