2020-10-07 03:00 AM
I am using STM32H743 MCU . I have interfaced a video camera at 25Hz. I am not using any video compression and sending the video data over ethernet. I have developed a software to see raw video which is also working. Now I want to convert this camera to ONVIF conformant camera. I am not able to compress video in STM32H743. Is there a way to compress video in STM32H743? For discovery and streaming I need 2 servers running on my STM32H743. Is it possible to do so without RTOS?
2020-10-19 05:16 AM
How can I compress raw video output to h.264 format in STM32H743.
2020-10-19 06:12 AM
You'd need to find and license a library capable of running on the platform