cancel
Showing results for 
Search instead for 
Did you mean: 

LwIP cannot be enabled

Ebun.1
Senior

Thank you for helping.

environment

STM32CubeIDE Ver1.3.0

STM32CubeMx Ver5.6.0

TouchGFX Ver4.13.0

board

STM32F769I-DISCO

The project made with TouchGFX was started with STM32CubeIDE.

Open STM32F769I_DISCO.ioc and select LWIP from category

Enabled cannot be checked in Mode.

Why?

Can TouchGFX and LwIP be used at the same time?

Thank you.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Hi @Ebun.1​ ,

Just Enable ETH ,then the Enable Lwip can be checked ,it is a condition for being able to access LWIP.

Best Regards,

Khouloud

View solution in original post

10 REPLIES 10
O. Mz. - 7
Associate III

Have a look at this http://ausleuchtung.ch/stm32-nucleo-f767zi-web-server/

It is not STM32F769 , but F767ZI. Still it is the F7 programmed with STM32CubeIDE Ver1.3.0.

Thank you for your reply.

It seems that what you introduce has nothing to do with TouchGFX.

Piranha
Chief II

Thank you for your reply.

Does that mean there is a defect?

Are they deadly?

Are you unable of reading even the title and the first sentence?

Khouloud ZEMMELI
ST Employee

​Hello @Ebun.1​ ,

Could you please share your ioc file ?

Best Regards,

Khouloud

Here it is.

Thank you.

Hi @Ebun.1​ ,

Just Enable ETH ,then the Enable Lwip can be checked ,it is a condition for being able to access LWIP.

Best Regards,

Khouloud

�?�返事�?�り�?��?��?��?��?��?��?��?�。

�?�?�り�?��?�。