cancel
Showing results for 
Search instead for 
Did you mean: 

Links to TouchGFX Documentation: Backend Communication examples not working

RReta.1
Associate III

Hello,

I want to download sample code from this page: https://support.touchgfx.com/docs/development/ui-development/touchgfx-engine-features/backend-communication

But I don't think the links are working, for example:

http://sw-center.st.com/touchgfx/TouchGFX/knowledgebase/hw_integration_tasks_exti.4.9.3.zip

Does not download the zip. I think the links maybe broken again.

Is there an updated link we can use to get the example code?

Thanks!

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Hi Romain,

Thanks for the response and hint! I was able to download from another browser.

The browser I was using was Chrome version 87.0.4280.141 (Official Build) (x86_64).

When it was not working, none of the .zip download links on the page seems to work.

/RR

View solution in original post

3 REPLIES 3
Romain DIELEMAN
ST Employee

Hi,

This is very odd as I am able to download it on my side. What browser are you using ? Do the other links work or is it only that one in your case ?

/Romain

Hi Romain,

Thanks for the response and hint! I was able to download from another browser.

The browser I was using was Chrome version 87.0.4280.141 (Official Build) (x86_64).

When it was not working, none of the .zip download links on the page seems to work.

/RR

Good to hear that you were able to download the zip you needed. I'll try to see if I can replicate that issue with the same Chrome version when I can just to check :ok_hand:.

/Romain