cancel
Showing results for 
Search instead for 
Did you mean: 

Integrating TouchGFX with I2C sensor

AVajd
Associate II

Hello!

I am working on to integrate a BMP180 sensor with my stm32f769i discovery board. The goal would be to read temperature and air pressure values and show these values on the screen. I have written the driver code in C for the bmp180 and it's working fine on other boards that doesn't use touchgfx, freertos, cpp. But it isn't working on stm32f769i with touchgfx on it.

I tried to use:

 extern "C"

{

   #include "bmp180.h"

}

But I get the following error:

Linking TouchGFX/build/bin/target.elf

TouchGFX/build/ST/STM32F769I-DISCO/Core/Src/main.o: In function `main':

c:\TouchGFXProjects\HWButton/Core/Src/main.cpp:153: undefined reference to `BMP180_Init(__I2C_HandleTypeDef*, unsigned char)'

collect2.exe: error: ld returned 1 exit status

gcc/Makefile:330: recipe for target 'TouchGFX/build/bin/target.elf' failed

make[2]: *** [TouchGFX/build/bin/target.elf] Error 1

gcc/Makefile:326: recipe for target 'generate_assets' failed

make[1]: *** [generate_assets] Error 2

../gcc/Makefile:45: recipe for target 'all' failed

make: *** [all] Error 2

Could you please help me how I can integrate my driver code and run it successfully? 

Thank you very much in advance!

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
cameronf
Senior

Can you post your "main.cpp", "bmp180.c", and "bmp180.h" files? It's hard to tell why linking is failing without seeing what's in those.