2018-12-31 8:45 PM
Hello all, I tried to integrate touchGFX to STM32CubeMX and I'm using keil to complie all the files. The complication is successful yet mountains of errors occurs during linking ! All errors are of the same type like this:
Error: L6654E: Rejected Local Symbol .x refered to from non group member x.o (.iar.stackusage)
Please help! I think I'm almost there!
Solved! Go to Solution.
2019-01-02 8:35 PM
The problem is finally solved. Here I will list the related procedure.
Hope this help.
Enjoy and goodluck!
2019-01-01 6:15 AM
Yes. This is a well known fact. Suggest to wait for the bugs to be fixed.
Please take some time to read the many related topics.
Full details on the exact procedure are now posted in this forum for:
STM32F429 with IAR + TouchGFX 4.10 + CubeMX 5.0
STM32F429 with SW4STM32 + TouchGFX 4.10 + CubeMX 5.0
STM32F746 with SW4STM32 + TouchGFX 4.10 + CubeMX 5.0
There are a few more but complete articles on the use of IAR with other targets on the parent Draupner website.
However, Keil support remains broken at this time of writing for the above combination of tools.
2019-01-01 6:05 PM
Thanks a lot for your comment. I agree that it might be a bug since L6654E is so rare that few solution is released currently.
I disabled touchgfx in STM32CubeMx and deleted all related c files. I enabled the framework again and the error comes to be:
"Error: L6242E: Cannot Link Object xx.o as its attributes are incompatible with the image attributes. ... wchart-16 clashes with wchart-32."
These xx.os are all touchgfx objects. Hence enum length definition conflict between touchgfx lib and STM32CubeMX library might be the reason.
I have to switch to AC6 compiler and use command line options to unify their length or just shift to IAR/SW4STM32 (which can be a better solution)...
2019-01-01 6:12 PM
If you can consider IAR, you will be in very good shape. Also, be cautious about which target you will be using as all of these tools are difficult to stitch together but the above models are stable.
< permanent link on our server >
2019-01-01 11:38 PM
Thank you for your sharing! It's rather impressive! I still worked on keil afterward and I switched to Arm Compiler Version 6.10.1. Here's the only error left:
469_touchGFX_interfacing_test\469_touchGFX_interfacing_test.axf: Error: L6683E: Merge Section TextFlashSection(texts.o) has an element size of zero
Furthermore, there're lots of touchGFX objects showing the warnings as below:
469_touchGFX_interfacing_test\469_touchGFX_interfacing_test.axf: Warning: L6776W: The debug frame in .debug_frame(stm32f4dma.o) does not describe an executable section.
as well as:
469_touchGFX_interfacing_test\469_touchGFX_interfacing_test.axf: Warning: L6869W: utils.o requested the Rogue Wave Standard C++ Library which has been removed from the product. This might cause link errors because libc++ is used instead.
2019-01-02 1:03 AM
I can load the images now! But still need some efforts to make touchController work...I found that keil users should generate the code and compile it at first, before pressing the execute button of touchGFX.
2019-01-02 8:35 PM
The problem is finally solved. Here I will list the related procedure.
Hope this help.
Enjoy and goodluck!
2019-01-02 8:42 PM
@Chi - many thanks for sharing!!
Your procedure may be the first working solution on this forum using the Keil compiler :)
Did you have to remove the duplicate LCD_Delay function?
Can you use the TouchGFX tool from STCube only 1 time or can repeatedly call from the GUI? My experience from a week or so ago was that you may use the GUI only once from STCube else all the work is reset to defaults. Perhaps an update has been applied already to fix this bug.
Will give this process a test when less tired. Thanks again!
2019-01-02 10:33 PM
Sure, LCD_Delay() in the discovery file is the one recommended to remove. I forgot to mention this stuff...
Sorry actually I think I misunderstood your description about the BUG, I had thought you mean If I execute touchGFX in STCube more than once the entire gui work would be erased (quite scaring if it's true) ! However after practice I found out you mean that all the settings of the widget in the project would be reset to default and unfortnately it also happens to me...The bug hasn't been fixed yet, my mistake.
Many Thanks to your effort on IAR and SW4 as well, or I may have difficulties in configuring the touch controller part!
2019-03-05 3:16 AM
How can I apply similar steps for stm32f746-DISCO ??