cancel
Showing results for 
Search instead for 
Did you mean: 

I want to set COLOR DEPTH to 24 Bit

Ebun.1
Senior

Thank you for helping.

environment:

board: STM32F769I-DISCO

TouchGFX 4.15.0

Is it possible to set COLOR DEPTH to 24 Bit?

If you can't, please tell me the reason.

Thank you.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Michael K
Senior III

Try following the reverse of the procedure outlined in comments of this post. YMMV.

If you are starting a new project, you can just use the 3.0.1 template, which uses 24bpp by default.

Embedded UI/UX Consulting: cadenza.design

View solution in original post

3 REPLIES 3
Michael K
Senior III

Try following the reverse of the procedure outlined in comments of this post. YMMV.

If you are starting a new project, you can just use the 3.0.1 template, which uses 24bpp by default.

Embedded UI/UX Consulting: cadenza.design
Ebun.1
Senior

Thank you for your reply.

I was able to realize it.

You're welcome. Did you follow the reverse procedure or did you use the 3.0.1 template?

Embedded UI/UX Consulting: cadenza.design