cancel
Showing results for 
Search instead for 
Did you mean: 

I'm using x-nucleo-gfx01m1 display with only TouchGFX.

FTrom
Associate II

 Using letters or numbers to create events, all works fine by selecting "Run simulation". If I want to use the joistick using the key 0 ,2, 4, 5, 6, 8 , nothing happened.

Thanks in advance

0693W00000D0J7XQAV.png

2 REPLIES 2
Romain DIELEMAN
ST Employee

Hi,

I am not sure I understand your question. What do you mean by "joist" ?

Are you working on a custom board with the x-nucleo-gfx01m1 display or on the STM32G0 nucleo board which its TouchGFX Board Setup is available in TouchGFX Designer ? Have a look at one of the Board Specific demos for the STM32G0 nucleo board to understand how to setup and use the joystick (or another hardware input in your custom board).

/Romain

FTrom
Associate II

Hi Romain, sorry for typing error. instead of joist i wanted to write joystick. It is on the board of  x-nucleo-gfx01m1 display. As a nucleo I m using Nucleo-G071RB.

In TouchGFX Config I cannot see how to set and I don't see any set up for external pins.

0693W00000D0KMJQA3.png