cancel
Showing results for 
Search instead for 
Did you mean: 

I have a 4.3inch TFT panel without built in controller.Want to drive it with MCU without graphic controller

bugur
Associate

.I want to drive it directly with stm32f469 LTDC . I do not want to put a display controller like SSD1963 or ILI9341 between TFT and the mcu.    Is it possible ? If possible , What is weak points of such design ?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
waclawek.jan
Super User

> stm32f469

The 'F469 has a MIPI/DSI output, it's probably not what you want. You probably want the 'F429.

> What is weak points of such design ?

Internal buses bandwidth.

Usually you'll need external memory which costs you extra pins.

Read AN4861.

JW