Skip to main content
Junde
Senior III
May 24, 2024
Solved

How touchGFX read the image from image.bin stored in SD card?

Hi all,

According to the document, I already store my image data to SD card and I can read the image data correctly by below function:

 

FRESULT read_bin_file(char *name, uint32_t offset, uint32_t numBytesToRead, uint8_t* dest)
{
	fresult = f_stat (name, &fno);
	if (fresult != FR_OK) {
		SD_ERR("\"%s\" does not exists\n", name);
	 return fresult;
	}
	
	fresult = f_open(&fil, name, FA_READ);
	if(fresult != FR_OK) {
		SD_ERR("opening file \"%s\" err[%d]\n", name, fresult);
		return fresult;
	}
	
	uint32_t numBytesRead = 0;
	f_lseek(&fil, offset);
	f_read(&fil, dest, numBytesToRead, &numBytesRead);
	if (fresult != FR_OK || numBytesRead != numBytesToRead) {
		memset(dest, 0, numBytesToRead);
		SD_ERR("read bin file \"%s\" err[%d]\n", name, fresult);
		f_close(&fil);
		return fresult;
	}
	
	fresult = f_close(&fil);
	if (fresult != FR_OK) {
		SD_ERR("close file[%s] err[%d]\n", name, fresult);
	}
	return fresult;
}

 

 I rewrite the TouchGFXHAL::blockCopy() function as below:

 

bool TouchGFXHAL::blockCopy(void* RESTRICT dest, const void* RESTRICT src, uint32_t numBytes)
{
	if ((uint32_t)src >= 0x70000000 && (uint32_t)src < 0x78000000)
 {
		LOG_DBG((char*)"read %d bytes at 0x%08x ", numBytes, (uint32_t)src);
 uint32_t offset = (uint32_t)src - 0x70000000;
		Mount_SD("");
		FRESULT res = read_bin_file((char*)"IMAGE/images.bin", offset, numBytes, (uint8_t*)dest);
		Unmount_SD("");
		if(res == FR_OK) {
			LOG_DBG((char*)"OK\n");
			return true;
		} else {
			LOG_DBG((char*)"err[%d]\n", res);
			return false;
		}
 } else {
		LOG_DBG((char*)"read %d bytes at 0x%08x", numBytes, (uint32_t)src);
 return TouchGFXGeneratedHAL::blockCopy(dest, src, numBytes);
	}
}

 

 After compiler and flash the program, however, the display can NOT show the screen, and there is nothing LOG output.

Does the blockCopy() NOT be called normally?

Can anyone give me some ideas, Thanks! 

This topic has been closed for replies.
Junde
JundeBest answer
Senior III
May 25, 2024

Not only should we store the image on the SD card, but we also need to get the image from the SD card actively.

Refer to the Document Here and the Video Here.

4 replies

Junde
JundeAuthor
Senior III
May 24, 2024

The map file info:

Junde_0-1716542411255.png

the read_bin_file() test result:

Junde_1-1716543300211.png

Junde
JundeAuthorBest answer
Senior III
May 25, 2024

Not only should we store the image on the SD card, but we also need to get the image from the SD card actively.

Refer to the Document Here and the Video Here.

June 2, 2024

If you you use SDRAM it's better to replace your image to the address of your pervious image. 

Just read the image file then set the address 

At the start of image address in the SDRAM

For example,  0xD0789000

This is work for PNG format and same size images 

Junde
JundeAuthor
Senior III
June 3, 2024

Hi @unknown 

My board has an external SDRAM, and I think the SD card is just for storing the image data for non-volatile.

Each time the system power on, the touchGFX will read the image data to SDRAM, and keep it for later access.

This is finished by "void Bitmap::cacheAll()"(if the SDRAM is enough), or "bool Bitmap::cache(BitmapId id)"(if the SDRAM is not enough for all the images).