cancel
Showing results for 
Search instead for 
Did you mean: 

How to sync progress bar and time running below in TouchGFX UI?

jsalg.1
Associate III

Hi,

I am beginner to TouchGFX , currently I am working on implementation of progress bar. requirement is I have to show progress bar based on user inputs. for example, if I have received 5 second as input, I need to show time increment and accordingly progress bar has to show progress. and at the end both timer and progress bar should complete the process at same instant.

Any suggestion about what best way is to implement this.?

Thanks in advance.

Regards,

jsalg.

 

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1

Hello @jsalg.1 ,

There are multiple tutorials and an example in TouchGFX designer that shows how to use a progress indicator. You can read about them here: 

https://support.touchgfx.com/docs/category/progress-indicators

I hope this would help you.

Mohammad MORADI
ST Software Developer | TouchGFX