2019-04-11 10:32 PM
I am creating my menu using ListLayout Example of TouchGFX example code.
I want to set the Limit of the Scrollbar. But when I reviewed the current example and Class, I could not find that part.
How can I set Limit ?????
The end of the current list is similar to the one below, but I want to make the end of the list like the second one.
1st.
2nd.
2020-10-15 02:01 AM
Hi Martin,
even applying the workaround you proposed I can't get the list not scrolling beyond the last element.. the list still scrolls beyond of a delta equal to one element height (instead of 4 elements height as it did with the original settings).
I see this post is not that recent, is there any update on the subject, in other threads maybe?
Thank you