cancel
Showing results for 
Search instead for 
Did you mean: 

How to modify TouchGFX source files in CubeIde ?

xth
Associate

I'm working on a STM32F469I-DISCO board. My project isn't difficult I think. I want to aquire datas with a radar and display some information on the screen in function (like distance between objects and later draw them at different places on the screen).

So now I'm using TouchGFX to configure the screen and I am importing the project in CubeIde to modify it and add my code related to the radar and the different calcul. Then, my objectif is to display information in the screen using "wildcards" that we can parameter in TouchGFX.

I've already see many tutorials such as this one https://controllerstech.com/touchgfx-5-data-from-uart-to-ui/ that I thought was exactly what I wanted, but it doesn't work.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello,

Refer to that link it could help you:

https://support.touchgfx.com/docs/tutorials/tutorial-06/tutorial-06-part-2

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
mƎALLEm
ST Employee

Hello,

Refer to that link it could help you:

https://support.touchgfx.com/docs/tutorials/tutorial-06/tutorial-06-part-2

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.