2021-03-13 2:37 PM
Hello ,
I am using STM32F429I-Discovery board I want to draw sprites on TFT-LCD with transparency on top of background image , I used black color as the transparent color for the images that I want to draw and used DMA2D at blending mode but the black color is not transparent and the sprite was drawn with a black color surrounding it.
the sprite color mode is RGB565 (I have tried ARGB888 also with no hope) .
The code :
void DrawSprite(uint32_t img , uint32_t SprNo , uint32_t w , uint32_t h , int format)
{
/* Configure the DMA2D Mode, Color Mode and output offset */
Dma2dHandle.Instance = DMA2D;
Dma2dHandle.Init.ColorMode = DMA2D_RGB565;
Dma2dHandle.Init.OutputOffset = 240 - w ;
/* Foreground Configuration */
Dma2dHandle.LayerCfg[1].AlphaMode = DMA2D_NO_MODIF_ALPHA;
Dma2dHandle.LayerCfg[1].InputAlpha = 0xFF;
Dma2dHandle.LayerCfg[1].InputColorMode = format;
Dma2dHandle.LayerCfg[1].InputOffset = 0;
if(SprNo == BACKGROUND)
{
Dma2dHandle.Init.Mode = DMA2D_M2M ;
}
else
{
Dma2dHandle.Init.Mode = DMA2D_M2M_BLEND ;
/* Foreground Configuration */
Dma2dHandle.LayerCfg[0].AlphaMode = DMA2D_NO_MODIF_ALPHA;
Dma2dHandle.LayerCfg[0].InputAlpha = 0xFF;
Dma2dHandle.LayerCfg[0].InputColorMode = DMA2D_INPUT_RGB565;
Dma2dHandle.LayerCfg[0].InputOffset = Dma2dHandle.Init.OutputOffset;
/* Configure DMA2D Stream source2 address */
WRITE_REG(Dma2dHandle.Instance->BGMAR, (uint32_t)RenderBuffer);
}
/* DMA2D Initialization */
HAL_DMA2D_Init(&Dma2dHandle);
HAL_DMA2D_ConfigLayer(&Dma2dHandle, 1);
if(SprNo != BACKGROUND)
HAL_DMA2D_ConfigLayer(&Dma2dHandle, 0);
/*DMA2D Transfer Start*/
HAL_DMA2D_Start(&Dma2dHandle,(uint32_t) img, (uint32_t)RenderBuffer, w, h );
HAL_DMA2D_PollForTransfer(&Dma2dHandle, 100);
}