cancel
Showing results for 
Search instead for 
Did you mean: 

how to drag and drop image from one screen to other screen in TouchGFX

Sgoti.1
Associate II

Hii,

i am working with STM32G474 MCU with 250X250 Pixel TFT display, i have Develop UI and it is working fine but now our code size is to increase so i want to make Generalize , so now i want to create one Screen and in that screen all the common image available and as per requirement i will access required image form other Screen , so can you please suggest how to move image from other screen to present screen,

i have try many thing but unable to do that ,

please suggest as soon as possible.

thanks

3 REPLIES 3
MM..1
Chief III

You can use one image more times, but generated is only one, then i dont see your idea? ...

Sgoti.1
Associate II

you means if I put same image in multiple screen then it is generated only once ?

Sgoti.1
Associate II

Hi MM,

I have check in TouchGFX, code size remaining's same if I used one image in one screen or multiple screen, but Due to modularity I want to know that how to access other screen image in presence screen,

I want to move /access other screen image in presence screen , so please suggest me best way.

thanks.