2021-11-12 9:21 PM
I am working on touchgfx LCD. I need a a support to develop our custom application.
i have seen touchgfx API functions setup screen but i need example for better understanding.
2021-11-13 8:20 AM
/*********************************************************************************/
/********** THIS FILE IS GENERATED BY TOUCHGFX DESIGNER, DO NOT MODIFY ***********/
/*********************************************************************************/
#include <new>
#include <gui_generated/common/FrontendApplicationBase.hpp>
#include <gui/common/FrontendHeap.hpp>
#include <touchgfx/transitions/NoTransition.hpp>
#include <texts/TextKeysAndLanguages.hpp>
#include <touchgfx/Texts.hpp>
#include <touchgfx/hal/HAL.hpp>
#include <platform/driver/lcd/LCD16bpp.hpp>
#include <gui/screen1_screen/Screen1View.hpp>
#include <gui/screen1_screen/Screen1Presenter.hpp>
#include <gui/screen2_screen/Screen2View.hpp>
#include <gui/screen2_screen/Screen2Presenter.hpp>
#include <gui/screen3_screen/Screen3View.hpp>
#include <gui/screen3_screen/Screen3Presenter.hpp>
#include <gui/screen4_screen/Screen4View.hpp>
#include <gui/screen4_screen/Screen4Presenter.hpp>
#include <gui/screen5_screen/Screen5View.hpp>
#include <gui/screen5_screen/Screen5Presenter.hpp>
#include <gui/screen6_screen/Screen6View.hpp>
#include <gui/screen6_screen/Screen6Presenter.hpp>
#include <gui/screen7_screen/Screen7View.hpp>
#include <gui/screen7_screen/Screen7Presenter.hpp>
#include <gui/screen8_screen/Screen8View.hpp>
#include <gui/screen8_screen/Screen8Presenter.hpp>
#include <gui/screen9_screen/Screen9View.hpp>
#include <gui/screen9_screen/Screen9Presenter.hpp>
#include <gui/screen10_screen/Screen10View.hpp>
#include <gui/screen10_screen/Screen10Presenter.hpp>
using namespace touchgfx;
FrontendApplicationBase::FrontendApplicationBase(Model& m, FrontendHeap& heap)
: touchgfx::MVPApplication(),
transitionCallback(),
frontendHeap(heap),
model(m)
{
touchgfx::HAL::getInstance()->setDisplayOrientation(touchgfx::ORIENTATION_PORTRAIT);
reinterpret_cast<touchgfx::LCD16bpp&>(touchgfx::HAL::lcd()).enableTextureMapperAll();
}
/*
* Screen Transition Declarations
*/
// Screen1
void FrontendApplicationBase::gotoScreen1ScreenNoTransition()
{
transitionCallback = touchgfx::Callback<FrontendApplicationBase>(this, &FrontendApplication::gotoScreen1ScreenNoTransitionImpl);
pendingScreenTransitionCallback = &transitionCallback;
}
void FrontendApplicationBase::gotoScreen1ScreenNoTransitionImpl()
{
touchgfx::makeTransition<Screen1View, Screen1Presenter, touchgfx::NoTransition, Model >(¤tScreen, ¤tPresenter, frontendHeap, ¤tTransition, &model);
}
2021-11-13 8:23 AM
1st screen is ok but for rest of the screens i did not get so how can i change my application from screen1 to screen 2 with out interaction. i need that give me support & concept.
2021-11-13 10:50 AM
OMG yes without interaction you need add this manualy to GUI files as everythink.
FrontendApplication.cpp
#include <gui/common/FrontendApplication.hpp>
FrontendApplication::FrontendApplication(Model& m, FrontendHeap& heap)
: FrontendApplicationBase(m, heap)
{
}
add here screen 2 3 4 ...
void FrontendApplication::gotoScreen2ScreenNoTransition()
{
transitionCallback = touchgfx::Callback<FrontendApplicationBase>(this, &FrontendApplication::gotoScreen2ScreenNoTransitionImpl);
pendingScreenTransitionCallback = &transitionCallback;
}
void FrontendApplication::gotoScreen2ScreenNoTransitionImpl()
{
touchgfx::makeTransition<Screen2View, Screen2Presenter, touchgfx::NoTransition, Model >(¤tScreen, ¤tPresenter, frontendHeap, ¤tTransition, &model);
}and into hpp ...
2021-11-13 11:13 PM
Thank you OK Is It works ? I will tell you after try manual addition.
Please tell about this stuff how to use beacause i am very new
Thank you but i have seen below information
switchScreen
virtual void switchScreen(Screen *newScreen)Switch to another Screen.Will call tearDownScreen on current Screen before switching, and subsequently call setupScreen and draw automatically for the new Screen.Parameters:newScreenA pointer to the new screen.
how can i use this to switch from one screen to other
virtual void switchScreen(Screen *newScreen)
2021-11-13 11:42 PM
maybe try
application().switchScreen( &Screen2View );
2021-11-14 7:04 AM
Hi
screen changing is working fine.
i have a doubt about buttons.
If i add any button with out interaction how can i know is that button pressed or not?
Is button operation work without button interaction?
2021-11-14 10:51 AM
Mark answer , that help you as best and open new thread for this question out of topic
2021-11-15 4:15 AM
ok can you please support for keypad widgets application.
i want to design keypad like mobile keypad
so how can i start to design keypad like custom smart mobile keypad.