cancel
Showing results for 
Search instead for 
Did you mean: 

How do you create an LCD project for STM32F769I-EAVL in CUBEMX?

HMoon.2
Associate

Hello

I have a question.

I have STM32F769I-EAVL board.

I can control LCD with TouchGFX.

But I want to create a project and control LCD with CUBEMX.

Is there a tutorial that controls (DSI) LCD through CUBEMX?

If not, could you tell me how to set up CUBEMX and control LCDs?

Thank you.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Imen.D
ST Employee

Hello @Community member​ ,

Have a look to AN4860 Application note: DSI Host on STM32F469/479, STM32F7x8/x9 and STM32L4R9/S9 MCUs, which contains : STM32CubeMX configuration example.

A set of example also are provided in STM32CubeF7 firmware package : STM32Cube_FW_F7_V1.16.0\Projects\STM32F769I_EVAL\Examples\LCD_DSI

Best Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen