2022-03-31 07:12 AM
2022-04-06 06:48 AM
Hello Mr. Berticus,
TouchGFX Designer does not support the snapper mixin, yet. But you can create your 3 position slide switch using the draggable mixin, for example with a box that can be draggable, and based on it position x, y you can implement the switch through code.
Or even easier, you can use the scroll list or scroll wheel with 3 elements on it.
/Osman