cancel
Showing results for 
Search instead for 
Did you mean: 

How can I create a TouchGFX Project with the STM32H7B3I-DK and write usercode with CubeIDE?

MMüll.6
Associate III

I have start with TouchGFX, select the demo board and generate the code. Simulator and download works.

But now, when I want open the project with CubeIDE, the first is, the project is completly empty. Then when I start a new project with the existing IOC file, then CubeIDE generate a seperate folder with other files, but there are not the auto generates files from TouchGFX visible.

What is wrong? Please write me step by step how can I start my own project with STM32H7B3I-DK.

Thank you very much, Markus.

11 REPLIES 11
MMüll.6
Associate III

Thank you very much!

Yes, now all works:

  • Debug with CubeIDE
  • TouchGFX Simulator
  • TouchGFX Download

I'm very happy!

/Markus

You're welcome :)

Osman SOYKURT
ST Software Developer | TouchGFX