cancel
Showing results for 
Search instead for 
Did you mean: 

Help connecting TouchGFX GUI with STM32F746 hardware

LevyCake
Associate

Hello everyone,
I am using a STM32f746 DISCO eval board. I am still trying to learn about this board but I have already done some small programs to get a feel for it and make sure that I can flash STM32CubeIDE and TouchGFX programs on it. Which I done successfully. However, I can't seem to figure out how to connect the two. I've tried watching some videos but I would like more direct help.

 

Goal: I have a CubeIDE program that sends a command through serial6/uart6 when the blue user button is pressed but the GUI remains pure white. I have a touchgfx program that has the button to press and can show up on the screen but does nothing with ports. I want the button on the screen to send my serial command instead of the user button on the board. How do I put everything together? Having trouble getting the generated code to the cubeide.

 

0 REPLIES 0